What is the maximum junction temperature of the PTD08A020W ?
The datasheet of the PTD08A020W, there is only a statement of the maximum ambient temperature. In addition, in the UCD9240 datasheet, there is a default over-temperature threshold of 100°C. Can I assume that the maximum junction temperature of the PTD part is 100°C?
Thanks