Dear Sir, please answer
I need 5 V supply, 2.5A current. Input voltage 25V. Temperature: minus 40 - plus 50 C, so I will use 150 µF output tantalum cap. I suppose to use LM2676-5.0 (260 kHz).
Point is that, I need to connect modules (from 1 to 10 pcs.) to my supply. Each module has 47 µF input cap (aluminum electrolytic), then total load cap may be 470 µF. This cap may cause unstable operation of LM2676-5.0? Probably yes.
What can I do? May be LM2596 (150 kHz) less sensitive to capacitive load? Earlier I used LM2576 (50 kHz) and I know, that it can withstand any cap load – I used 2200 µF and supply worked, but it has high spikes at the out and I could not get rid of them! Please, advise me anything
TIA
Sincerely
Vladimir Naumenkov
www.agat.by