Hi
I am using TPS54339 for converting 12V supply to 5V. Circuit has options for both 5V and 12V input power connectors. 5V connector is connected to output of TPS54339 after inductor. Circuit performs without any issue at 12V. At 5V, circuit performed without any issue but at random times, a 220uF tantalum capacitor placed at the 12V input of TPS54339 blows. There is no other damage to the circuit apart from this capacitor and once this cap is removed, circuit works find without any other part being touched. There is a protection diode (used 1N4148 ) before the capacitor in case there are some surges in 12V.
This happened on 4 different boards and same behavior was observed. I could not find any explanation of this tantalum cap catching fire when there is no direct Power. Please suggest what rework/modification can be applied to prevent further damages.
Regards,
Fahd