Hi,
I am planning to use TPS61021A to generate 3V3 from a single Ni-MH (classical AA battery let's say) cell. Light load efficiency is important for this application. Efficiency of TPS61200 seems to be worse than TPS61021A in my case. However unlike TPS61200, TPS61021A doesn't offer an adjustable UVLO threshold values. According to the datasheet of TPS61021A, it operates until the input is low as 0.5V. However to protect Ni-MH battery, I want to cut-off the operation around 0.9V or 1V. How can I achieve this operation? Should I use a comperator with hysteresis to disable TPS61021A via EN pin? In that case, I couldn't find a proper comperator due to low operating voltage limit (0.9V let's say). Could you give some suggestions? The operation temperature will be between -20C and 50C.
Thank you.
Alper.