Hi TI Experts:
For NiMH battery charger, BQ2002T and BQ24401 for multiple cells charging, does it has the Power Management Path??
I read through some products for Li-Ion, example the BQ24230, it has the power management feature.
(priority will be given to AC adaptor to supply to load when it present, else it will use the battery to supply the load)
The project will be using 3 NiMH is series to achieve 3.6V output voltage.
Thus, I have some inquiries for BQ2002T and BQ24401:
1) Will the IC will direct supply to the system load and the battery will start discharge when there’s no VCC supply to the ICs
2) Or once the battery is fully charge, both IC will not direct supply to the system load but instaed of the battery and till the battery is fully discharge, both IC will recharge the battery again and the cycle will repeat again?
Please advice.
Thanks,
Br,
Teach Me