I have designed a 3.3V DC-DC converter using the TPS62132 to drive an ARM Processor / display board. The maximum current in worst case condition should be 2A, but I have designed the DC-DC converter to be capable of supplying 3A. The board has been carefully designed as recommended in the application notes and data-sheets. I have tested the board with a static load and it works as expected. When tested using the processor board, there is an audible noise for a second or so during the processor board power up sequence. The board draws a peak current of 0.85A with a 6V supply, so the output current should be well below the maximum current. Can anyone suggest what might be causing the noise? To me it indicates that a component must be under some stress.