Hello,
For the purpose of failure rate calculations (as per IEC TR 62380), I need the transistor count for the ICs. An approximate is ok (such as "between 100 and 200").
The chips I'm interested in are: TPS65320, TPS62420, and TPS54618-Q1.
Even if the exact information is confidential, approximate values would do (for now, I'm putting what I think is a conservative estimate of 1000 transistors --- I think it should be much less than that, right?)
Thanks,
Carlos
--