This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27531EVM Update status0 Stuck at 1

I am following slu595, to perform a learning cycle.

I am using a Varta 3.7V 2400mAh liPo battery.

I start with a discharged and fully relaxed battery that is measuring 3.0V open circuit.

Issue an IT_ENABLE

Charge to Full

Update Status goes from 0 to 1.

Discharge at C/5 until empty.

Relax for > 5hours with no load, battery settles to 3.0V

Update Status never changes from 1.

Inside slu595, I do not see any suggestions as to why this could be happening.

Any help with this issue would be appreciated.