Team,
Our customer is considering TPS544B20 due to D-Capx and high output current, however they don't want to use PMBus interface.
The DS describes about "Default" setting, but I cannot find out any comment in it regarding no PMBus use case.
Could you please give any information that whether the device can use without PMBus interface.
If it can be done, how should we address both pins; CLK and DATA ?
<<Customer's Spec>>
Vin = 15V
Vo = 0.9V
Io = 20A
So they don't want to use neither voltage mode devices (due to load transient response) nor TPS548D2x (due to its 16Vim max limitation)...
よろしくお願いします。
Thanks and Regards,
Metropolitan (Tokyo) Area FAE Kenji Ninagawa