Hello,
I'm having a bit of a debate with one of our engineers here. We are attempting to drive a resistive load (0.5 Ohm) up to a maximum power of 18W. Our current boost circuit using the TPS61088 is designed for a maximum of 18W (9V @ 2A). We need to control the power going through the load from 0-18W.
Right now we have a second (buck) converter (STM LED2001) attached to the output of the TPS61088, which regulates the power as needed. However the parts count and footprint for 2 converters is large. My colleague is suggesting we remove the buck converter and just use the TPS61088, with the output connected to the load through a simple MOSFET switch, and the power output is controlled by PWM of the MOSFET.
Here is my concern with this: while the MOSFET is turned on, the 0.5 Ohm load on the TPS61088 @ 9V will try to draw 18A - 162W! Obviously the TPS61088 can't provide this, but it seems to me we are effectively shorting the output every time the MOSFET turns on.
So my question is - is this a safe way to control the power going to a low-resistance load? Or do we need to make sure that we don't exceed the power rating of the TPS61088 with external circuitry?
Thank you for any help!