This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please help me about non ISO DC/DC!

Other Parts Discussed in Thread: LMR12015, LM53601-Q1

Hello.
My customer is currently in considering LMR12015 or LM53601-Q1,now.

My customers would like to compare that devices.

If my customer have this data in one week later, the customer consider either of devices.

It will mount to a wireless transceiver system(For policeman).
I want to win this project.

So, please support me !

<Request contents>
Please give me the efficiency data of these two devices under the following conditions.

Conditions
Device:LMR12015 and LM53601-Q1
VIN:10.8V
VOUT:5.0V, 3.3V and 1.2V
IOUT:5mA, 10mA, 50mA, 100mA and 200mA
Fsw Setting:2.0MHz
Mode Setting:PWM only
Other peripheral BOM:EVM's recommended value

Could you help us?

Best Regards,Masumi Sekiguchi