This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4041C - Likely bad batch of LM4041CILP voltage reference

Other Parts Discussed in Thread: LM4041C

Part Number: LM4041C

Application: ref voltage for audio application

Question type: Production/quality issue

Support topic: /Feedback/Other feedback/

Description of the problem: As part of a recent order with Mouser I purchased 50 pieces of LM4041CILP. I've been using this same part in one of our products for almost 3 years with no problems. We use it to generate 1.8 volts. In recent builds using this part we started to notice that it was generating only 0.7 volts rather than 1.8 volts. We've made not made any hardware changes and we double checked that all other parts used with this part are correct.

As part of our troubleshooting we replaced the part with the exact same part number but from a different batch of identical parts bought under a prior order. Replacing the part corrected the voltage problem.

The only reasonable conclusion we can make is that this most recent batch of LM4041CILP voltage reference parts are mostly faulty or fail soon after being installed.

Using a hi-rez scope the data on part are as follows:

51ML50E
NPCI
TI

According to TI docs the NPCI is the code for the part LM4041CILP.

This part is critical to our product and we are being delayed due to this problem. We have provided similar notice to Mouser.

  • Hello Morten,

    Thank you for the heads up. Please follow the appropriate channels through Mouser and they will support.

    Best,
    Michael
  • We managed to resolve this problem by changing one of the resistors values that we used with this voltage reference. This increased the current through the reference which caused it to perform normally as before. Prior to making this change we had previously produced close to 400 units with this voltage reference with no problems. Even thought the technical specs on the voltage ref did not change, apparently changes in the manufacturing tolerances resulted in it no longer working properly with the resistors/current we had been using.
  • Hello Morten,

    Glad you were able to figure it out. If you designed the cathode current close to the limit, then you may see this issue. Generally we recommend some cathode current margin to ensure voltage regulation over temperature, system, and process variation.

    Please feel free to reach out on E2E again in the future. Although I know it took some time to get back to you on this, we strive to have 24 hour response times on these forums. This forum was recently setup, so my apologies for the delay in response.

    We are constantly monitoring these forums to provide the best support we can, so I encourage you to continue to post here.

    Best,
    Michael