Hi all
Would you mind if we ask LMR61428?
The datasheet shows the following;
While tantalum chip capacitors are recommended for the input and output filter capacitors, ceramic caps can also be used.
Is it possible to use 47uF x 2 ceramic capacitances for output capacitance?
Is there define about ESR for output capacitance? Only "Very high ESR values (>3Ω) should be avoided."?
Kind regards,
Hirotaka Matsumoto