Hello,
I have a question about how to understand the specs of parameter "Switching frequency" of TPS54388-Q1. It says 200 (Min) to 2,000 kHz (Max) as the "Switching frequency range using RT mode." Please let me take an example, if switching frequency variation including device performance and RT resistance were ±10% and the actual frequency must not exceed 2 MHz, do I have to set the nominal switching frequency in design to 1.818 MHz or lower? Or, do the data sheet specs indicate that the nominal switching frequency can be set up to 2 MHz and the device will work at frequency above 2 MHz due to variation?