Dear Sir/Madam,
We purchased TPS61235P boost up converter that is we got efficiency only 60 % and also have some problems.
1. At 3V input, circuit drawing 1A input current and 380mA output current at 4.8 V output.
2. After 1A input current means i am varying load resistance than device goes to shutdown.
So please give some suggestions to rectify the problems.
Thanks and Regards,
Sowjanya