This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Michael,
I got a little bit confuse for this description here "The input inductande ist 22µF, the output has 47µF, than an ferrite and again 4x47µF MLCC to stabilize the supply for the VCSEL array." Is 22uF and 47uF for input and output inductor or for capacitor? The unit for inductance should be H. I think you want to mention the input and output capacitor. TPS563200 is a DCAP2 part which require low ESR output cap in application. It is different from the DCAP part which require high ESR cap. There is no need to have a large output ripple for stability since there is internal ripple injection. In this case, the low ESR cap is recommended. It is for the stabilityt.
Best
Anthony
Hi Michael,
I did not see any issues with stability if using higher DCR. If higher DCR indcutor selected, which means lower quality factor filter, the damping factor will be bigger. It only leads to smooth change of phase around resonant pole on bode plot. For DCAP2 part, there is a zero placed after resonant pole by ripple injection that will boost phase towards 90 degree. In this case, the phase will have enough margin around crossover frequency. No stability issue but only lower efficiency will have if bigger DCR inductor is selected.
Best,
Anthony
Hi Anthony,
thank you for the explanation. This will help me.
Best regards
Michael