Hi:
I have built a 5V high side buck converter around the UCC28880 almost identical to the circuit in EVM-616. This shows a stable output under low load but a sawtooth oscillation under 50mA load. Looking at the datasheet, equation 19, I see that there could be a potential problem with the time constants. That equation says that the time constant Cfb X (Rfb1 + Rfb2) should be about a tenth of the time constant CL X RL, because the voltage across Cfb is not updated in real time. I also see that the evaluation board EVM-616 schematic has been designed that way. However the catch is that the RL X CL time constant obviously changes as soon as you connect a load and therefore this 1/10 relationship falls apart. . In my case the numbers are as follows:
Rfb1 = 39k, Rfb2 = 9.1k (output = 5.4V), Cfb1 = 2.2uF. CL = 47uF, RL = 10k
This gives me a value of 105ms for Cfb X (Rfb1 + Rfb2). The moment I connect a load that draws 50mA, RL has effectively dropped to 100 ohms. Now the
RL X CL time constant is 4.7ms and that means that the time constant of 105ms is way too high: it should be a tenth of RLXCl = 0.47ms! The datasheet says that if Cfb X (Rfb1 + Rfb2) is too high then the output voltage may drop. Perhaps this is what is happening - drastic drop in output voltage followed by an attempt by the feedback loop to pull it back up etc.
Can A TI engineer help with this formula which apparently seems to break down in this case? What am I missing?
Thanks - Ram