Hello
LM27761 negative voltage converter has an excellent performance but the WSON-8 package is tiny for trial PCB (i mean that the device will be soldered with hot air at workbench). I tried many times to locate an equivalent (i need -2.5V / 150mA output for a Vin=5Vdc, i.e. the Vbus of USB input) in other package without success. Is there any equivalent part in e.g. SOIC-8 package?
Thank you!
Fotis Anagnostou