This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8725 I2C address clarification

Other Parts Discussed in Thread: LP8725

Hello all,

Table 1 shows the I2C address of this device based on CONFIG and DEFSEL pins. The four possible 7-bit addresses are:

   0x78;  1111000_

   0x79;  1111001_

   0x7A;  1111010_

   0x7B;  1111011_

      Note: "_" is supposed to represent the R/W bit

These I2C addresses seem to be reserved according to the I2C specification, yet there are Linux drivers so I assume things are working fine. I can not find an evaluation board to buy and verify for myself.

Seems that I2C addresses 11110xx_ are supposed to be ignored by 7-bit I2C slaves; used for 10-bit addressing.

Additionally I2C addresses 11111xx_ are supposed to be reserved for future use.

 

Can someone clarify the I2C addressing?

Is the LP8725 not compliant with I2C Specification wrt slave addressing?

 

Regards,

Steve