Could someone elaborate on what would happen if you loaded a boost cap (the cap connected to pin 3 and the high side switch) that was too low. I accidentally loaded a 470pF instead of a 470nF and am wondering if this could damage the part. I saw a lesser output voltage (~3.0 instead of 3.5) on the output. After replacing the part it looks like it is running fine. I'm just wondering how much risk is involved in not replacing this part. Would this be a major cause for concern?
Also, why is there a charge pump necessary for the high side switch?
Thanks!