This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28700 and UCC24610 PMP design dimensions

Hi,

What are the dimensions (W x L x H) of PMP8965 and PMP4351? 

Thank You,

Mike 

  • Mike

    For PMP8695, the X-Y dimensions can be read off the pdf version of the layout on the web page under "download design files":
    www.ti.com/.../tidc842

    This board is 42 x 57 mm.

    The max height component is C4 at 14 mm, this info is contained in the Altium design files, also available under "download design files".

    Allowing for 2.5 mm SMT component height under the PCB and 1 mm for PCB thickness, overall assembly height is 17.5 mm max.


    For PMP4351, the dimensions are not included in the gerber pdf on this one, and the original Altium files are not available to download.

    However, I have checked internally and the dimensions are as follows:
    27 x 41 mm PCB X-Y size.

    Max height 13 mm above board, 2.5 mm under, so max assy height ~ 16.5 mm (allowing 1 mm for PCB thickness).


    I hope this answers your questions, if so please click the "verify answer" button.


    Thanks,
    Bernard