This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54427 inductor selection?

Hi Sir 

Due to my customer want fix inductor at 4.7uH(DCR=0.04ohm/Irms = 5.5A Isat is 10A).

application is 12Vin to 5V/3A and 12Vin to 3.3V/3A.

I run wench bench. the 5 Vout/3A can be use. but 3.3V seems no recommend.

and i see DS that inductor should be match output capacitor. but i can't find match 4.7uH data. 

May you pls have suggestion for us?

                                              Bogey