Other Parts Discussed in Thread: TPS53647
Hi,
I am running the TPS53647 as a 2-phase 35A design.
Section 7.5.1.10 says to connect CSP2, CSP3 or CSP4 to V3R3 to select the maximum active phases. Table 3 says that I can connect CSP3 to V3R3 for 2 active phases.
There are two interleaving modes supported, “4 phase individually” and “1/3 and 2/4 phase interleaving”. I can’t find any explanation for what 1/3 and 2/4 interleaving means.
I currently have CSP3 connect to V3R3 with a pull-up.
My assumption is that phase 1 and phase 2 are going to be interleaved.
1) Should CSP3 be connected to V3R3 with a pull-up or direct? It doesn’t say.
2) Am I correct that phase 1 and 2 will be active?
3) What does 1/3 and 2/4 interleaving mean?
Thanks,
David