This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28089: softstart of UCC28089

Part Number: UCC28089


Hi,

I want to make a soft start so that no inrush current will occur at UCC 28089.
Is it possible to add soft start function with this device?

The structure is a half bridge. The control IC on the secondary side is not used. The IC is only on the primary side.

Best Regards,