This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: Use LM5175 with variable output voltage / output current

Part Number: LM5175


Hi

I want to use LM5175 to charge a battery at constant voltage and current

I also need to be able to set the output voltage and output current variable.

Is it possible to use an external operationnal amplifier to adapt the regulation at the level I need and to go directly to COMP pin.

That means NOT using internal LM5175 amplifier with 0.8V threshold

Thanks in advance for your answer

Xavier