I'm switching the TLC5917s' Vdd to minimize the quiescent current of the TLC5917s when no loads are active.
Question: How long after applying Vdd does the MCU have to wait before starting to clock data in.
Details: -OE is held at Vss. Six devices are cascaded. Clock frequency is 250 KHz. Vdd is 3.3v, Vled is 5v, Current is 12 ma. but the LEDs have resistors to Vled to minimize power dissipation in the TLC5917. Special Mode is NOT used.
The MCU currently applies Vdd and then waits 5 ms. before starting to send the serial data. There are no issues, but I'd like to reduce that time, hopefully to a few microseconds. I just didn't find documentation on the initialization.
One option is no delay, but send seven (7) bytes of data for the six (6) TLC5917s. The first byte would be all zeros and hopefully would be ignored. But if startup is fast enough, I can avoid the wasted time.
Thanks, G. Peterson