Other Parts Discussed in Thread: AM5728, TPS3808
Hello,
We have a design based on TMDXIDK5728 using PMIC TPS6590377 and AM5728. The board is intended to be always ON so we implement the "imminent shutdown" circuitry with TPS3808 voltage monitoring (based on schematic AM571_IDKEVM_Page5Rev1_3A).
During preliminary testing TPS3808 circuitry was not available and the boards have been turned on/off with a switch toggling imminent_shutdown signal between 0V and 5V (Pin is 5V tolerant).
Now, we are using the following design on the same boards:
On some of the boards (At least 3 on 5):
- The imminent_shutdown signal is stucked to ground and the board does not start
- If imminent_shutdown signal is floating (pull up to VRTC_OUT), the board does not start
- If I force imminent_shutdown signal to 5V, the boards starts
Some of the boards start correctly (At least 1 on 5).
We suspect the switch to have produced overshoot and/or undershoot on pmic_reset_in pin and damaged the component. We are going to replace a PMIC to validate this assumption.
Questions:
- Can undershoot/overshoot on PMIC_RESET explain damage on component?
- Because the same problem occurred on several boards, do you think something else could explain the failure?
Thank you for your guidance.