Part Number: BQ25071-Q1
Hello,
Looking on the bq25071-Q1, I have a LiFePo4 3300mAH Battery 3.2V with cahrging float at 3.6V, also I have system load of 340mA
I was wondering if I set ISET for 1000mA Charging and leave it set as this, what will happen if the charger IC is connected to a USB power which is only providing:
5V at 100mA
or
5V at 500mA
or
5V at 1500mA
Am I correct in thinking that the Charger IC will take what it can and pass it onto the battery and switch off the system load if its too little?
Best regards
Mo