This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

12V to 3.3V isolation power



Hello,

            Do we have 12V to 3.3V isolation power and reference design for customer? Thank you. 

BR
Patrick

  • how MUCH power? and how CHEAP? the PA3856.004NL from PULSE is reasonably inexpensive ($3.50 each, $2.00 @ 100, etc) and can supply 3.3V@10A from 12V@200KHz flyback in roughly a 0.500" cube off the shelf
  • Patrick,

    As Dan said, can you specify your required power level?

    You can search all available TI-Designs and reference designs here:
    www.ti.com/.../refdesignsearchresults.tsp

    You can click on the tab "Search power designs by parameters", then refine your search by input voltage range, output voltage, output current, DC/AC input, isolated/non-isolated, etc.


    E.g. if I search for isolated, DC-input, 10-14V input range, 3.3 V output, i get 47 results, ranging in power from 57 mW to 96 W.

    There is likely to be a design in that list that comes close to your spec.

    I hope this helps answer your question, if so please click the "verify answer" button.

    Thanks,
    Bernard