Dear *,
where can I find Ien(max) of TPS62170-Q1 in the Datasheet?
I want to calculate PGpull-up max and PGpull-up min value as in the SLVA485-October 2011.
I do a power sequence so that one TPS62170-Q1 PG pin is driving EN of second TPS62170-Q1
In order to calculate the Rpull-up max as
Rpull-up=(Vout-Vih)/(Ipull-up) => Ipull-up= Ien + Ilkg
And to calculate Rpull-upmin I need the iOL -> I can use the 2mA for this from The DS?
Best Regards.