Hello,
If I design my circuit just as the insert file,whether will TPS61040 be damaged or not when without load?
Waiting for your help,thanks!tps61040_without load.docx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
If I design my circuit just as the insert file,whether will TPS61040 be damaged or not when without load?
Waiting for your help,thanks!tps61040_without load.docx
as your output voltage is 9.3V, so please choose R1=634k, R2=97.6k, Cff=22pF.
do you mean you will add several LEDs between Vout to FB? or the output voltage will get very high and cause damage!
then you can refer to the document : slva227 for the over volatge protection solution if you are worries about the LED failure.