This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24190: Fast Charge using BQ24190 and standard Qualcomm power adapters

Part Number: BQ24190
Other Parts Discussed in Thread: BQ25890H, BQ25890

I understand from the datasheet that the BQ24190 can provide up to 4.5A of charge current through the use of a high voltage adapter.

What I have not been able to clarify my customer is how to use the device with a standard dual voltage phone charger, such as qualcomm/samsnung models, in which the default output voltage is 5V, but upon negotiation, the device raises the output voltage to 9V.

Is there an aditional device to perform this autentication or perhaps a different controller that supports it?

Many Thanks.