This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65233: TPS65233 current set and 5V efficiency

Part Number: TPS65233

Can the TPS65233 be set to current limit at 100mA?

What is the boost efficiency from 5V input source to 100mA out?

  • Hello David,

    The selectable current limit is a function of the LDO on the VLNB pin not the boost converter. The boost converter does cycle-to-cycle current limiting based on the switch current limit which is not a settable value.

    The efficiency of the boost converter is very dependent on the input and output voltage and the output current. Right now it is hard to say with only the input voltage of 5V and 100mA