Part Number: UCC38C43
Hello,
The reference voltage inside the UCC38C43 controller is said to range between 4.9V to 5.1V.
The internal error amplifier of the UCC38C43 is presumably supplied from this reference voltage, so how is it that near the bottom of page 5 of the UCC238C43 datasheet, it states that the output high voltage (VOH) of the COMP pin ranges up to 6.8V?
The “Test Conditions” for this voltage (6.8V) is said to be…….
“VFB = 2.7 V, RCOMP = 15 kΩ COMP to GND”
…however, if the FB pin had 2.7V on it, and there was a 15k resistor to ground connected to the COMP pin, then the COMP pin voltage would tend to be near zero volts.
Also, page 2 says that the COMP pin's "Absolute Maximum" voltage is just 6.3V.....so how can it have 6.8V on it like on page 5?
Do you know what’s going on?
UCC38C43 datasheet:
http://www.ti.com/lit/ds/symlink/ucc38c43.pdf