Other Parts Discussed in Thread: BQ24035
Hello,
Does bq24032A have OVP or overcharge protection function?
I couldn't found the description about these function.
Best Regards,
Ryuji
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ryuji
OVP:
The USB recommended max input voltage is 6V with absolute max of 7V.
Max AC input is 16V with absolute max of 18V
The bq24035 has AC input cutoff protection, at 6.4V the AC input FET will disconnect input.
Overcharge Protection:
Max Output voltage is regulated to 4.2V with +/- 1% accurate over temp
Charge current for all phase of charge is controlled by the device, set by ILIM1/2 pin
Timer will limit charge duration, set by resistor on TMR pin
TS pin available for Batter NTC to limit thermal rise.