Hello,
I need to create a 0.8V output. Can I use feedback resistors on the LM3691TL-0.75 device to generate the desired output voltage?
Don
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I need to create a 0.8V output. Can I use feedback resistors on the LM3691TL-0.75 device to generate the desired output voltage?
Don
Hey there,
Looking forward to a response.
Don
it's not ideal, cause this device was not designed for adj output. but since you only want move 0.5V, it should be ok, only draw back i can think about is the vout accuracy may get worse since the R tolerance is different.