Other Parts Discussed in Thread: TPS61230
Hello,
I read that one can use a voltage divider hooked up to the EN pin to automatically disable it when my battery is at 3V. I am having trouble figuring out what resistors i will need for this application.
Could someone please advise me on what voltage divider resistors I should use, or if this in fact the best solution?
I don't want to drain the battery even lower after cutoff occurs with incorrect resistors that would allow too much current to flow into the EN pin.
I am using the WEBENCH schematic. I have attached a picture for convenience sake.
Thanks so much!
Dillon