This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC5925: IO and VO Characteristics

Part Number: TLC5925

Hi all.

I have two questions.

1.How much is the maximum output cuttent at Vo>0.6V.
   Is it 45mA?



2.There is output current - output voltage graph in the datasheet.
   I attached the following,
   The temperature of this graph is 25℃
   I would like to know the output current - output voltage graph at 50℃
   Can I refer to the following graph when Ta= 50℃?


Best Regards,
Sho