Hi all.
I have two questions.
1.How much is the maximum output cuttent at Vo>0.6V.
Is it 45mA?
2.There is output current - output voltage graph in the datasheet.
I attached the following,
The temperature of this graph is 25℃
I would like to know the output current - output voltage graph at 50℃
Can I refer to the following graph when Ta= 50℃?
Best Regards,
Sho