Hi,
I'am using BQ34Z100-G1 on BQ34Z1xxEVM and EV2300 adapter.
I'm trying to set up the correct registers values for a pack. i'am struggling with the following values :
Configuration/Data/Design Capacity
Configuration/Data/Design Capacity
My pack is a 1S8P LiFePo4 assembly (8 x 18650 1500mAh LifePo4 cells)
Nominal voltage 3.3V
Nominal capacity 12.8Ahr
Nominal energy 42.24 Whr
As a first approach, I used Chem ID 0426 (not the exact brand/model, but seems close enough at first sight)
The datasheet is stating that max supported battery capacity is 29Ahr, so I should be ok on this point and set for my case '12800'
However, the field Design energy seems to be limited to a maximum value of '32767' (mWhr) as per the datasheet.
Is there something i did'nt get, or I cannot sense the whole energy capacity of my battery pack with the BQ34Z100-G1 ?
I did'nt run the optimisation cycle yet, but assuming I run it, can I get a Qmax value bigger than the 'Design Energy' value ?
Thanks for your help
Regards