Hi
I want to know about OVP condition of bq51020.
below comment is in datasheet of bq51221. Is it apply to bq51020 equally?
- bq51221
Over Voltage : 0x04 : VRECT target does not converge(3)
(3) If the voltage on the RECT pin does not reach the required value (typically 8 V) within 64 error packets
during startup (weak coil coupling), the receiver sends EPT-OV and the transmitter will shut off.