This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563209: TPS563209 Inrush current limit

Part Number: TPS563209
Other Parts Discussed in Thread: TPS54328

Hi Non-lsolate DC/DC team

We measure to need Inrush current limit on TPS563209-EVM for SetTopBox Application

Can we get really production test result as a blow?

[Vout=5V, L1= 4.7uH]

We test to have OCP(Over Current Protect) function as a picture.

[Load: 400mA, Pick to Pick current: 4A]

However, TPS54328 don't have OCP function despite same spec(TPS563209)

  

And, We will use TPS563209 continuously

Can we get really production test result that Vout=5V, L1=4.7uH ?

Do you have solution for OCP solution?

Thanks

Best Regards

Gerald.