This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2991: Output leakage current is changed

Guru 20090 points
Part Number: LM2991

Hello

Output leakage current of LM2991 is changed from 250uA to 150uA in Revision I.
However there is no description in the revision history.
Which specification is correct?


 

Best Regards,

Ryuji

  • Hello Ryuji,

    Thank you for bringing this to our attention.

    The correct LM2991 MAX Output Current Leakage value is 250µA.

    I have submitted a request for an expedited correction to the datasheet.

    The updated LM2991 datasheet should be on-line within 24 hours.