Other Parts Discussed in Thread: PMP10948, UCC28180, UCC28070
Dear Sir
I am trying to design an 1.5KW PFC using UCC28063A power rating please below
input range : 85~264Vac
output voltage : 390V / 3.85A
And I have refer PMP10948 before,but I want to design 1.5KW in one power stage.
PCBA is complete and on testing, but when Vac 115V and output power over 900W,
Vout will drop from 390V to 342V.
Could you give me some opinion to solve this issue.
some parameter for you reference.
Rtset = 121K
Rs = 0.001
L1=L2=160uH
Many thanks!!