I would like to know the possibility of the following problem.
Under the condition that TPS3839 IC is being exposed to strong light such as laser pointer or 850nm light (less than 1mW), when Vdd is set more than threshold voltage, I found the problem that the reset signal doesn't become "High" l after some delay.
Once the reset signal become "High" after Vdd on, the reset signal keeps "High" when IC is exposed to strong light after that.
It would be appreciated if there is some information and mechanism of such problems.
Best Regards,
N Nakamura