Other Parts Discussed in Thread: TPS54232, TPS54233EVM-373, TPS54233
Hi team,
We are interested in using the TPS54232 in an application to buck 18V down to 15V for a 1A load.
Looking at the EVM for this part, it says the input voltage range is only up to 15V even though the part is rated for 28V. Will there be an issue with using this EVM for 18Vin? Do I need to make any modifications to make it work for this? It looks like I will have to change R6 to 575 Ohm according to Formula 1 in the EVM User's Guide.
Also, are there any other/better parts that we should be looking at for this application?
Regards,
Akash Patel