This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Getting error when importing parameters in BQstudio

Part Number: BQ34Z100-G1

Hi. We are buying battery packs from a manufacturer, but we want to edit the parameters of the fuel gauge that is in this battery packs, but we are running into a problem.

For ease of use we want to import the parameters from csv file. I will describe the steps I did so it is easier for you:

1. opened the bq studio with the battery pack connected

2. edited the parameters

3. exported the parameters to csv file

4. imported the parameters 

5. tried to write all and got this:

I did not change the CC Delta so this seems strange. I attached the csv file too. Maybe you can help me?

Thanks in advance.

battery parameters.rar