Hello,
I am looking at using the LM5119 in an application with dual 24VDC 4A (100W) outputs. We want to create a single PCB assembly which can be figured with jumpers for two seperate 4A channels, or a single 8A channel.
What's not clear to me from the datasheet is how this affects the compensation calculations. As an example, if I have 100uF of output capacitance on each channel and bridge them together, this yields 200uF output capacitance. It seems this throws off the equations used to calculate compensation. Will I need to remove one of these if I jumper the outputs?
Thanks,
Dan