Hello
I have a question about TPS54561-Q1 output capability.
In our design, we need current having 5.3A output capability.
And we try to use TPS54561-Q1.
However this regulator could support 5A output capability which could be found in the datasheet(in Tittle and Description epsoide).
-
Is ‘5A’ the limit of output capability?
-
To get more output current capability, we try to increase the inductance , so we could get lower ripple current so that even average output current is 5.3A ,the peak current through Switch MOS will not exceed the 6.3A. Is that possible?
-we will comply with the datasheet that the minimum ripple should be greater than 150mA.
Some information about our application:
Input:16-36V
Output:3V3
Operating switching freq:1.5MHz
Load current (worst case):5.3A