Part Number: TPS61241
Other Parts Discussed in Thread: TPS61240
Hi! I have two questions regarding the TPS61241:
1. If there is a hard short on the output, what is the expected behavior?
-How much current will the device supply?
-Will it run continuously in current limiting mode?
-Will the device only shutdown if it reaches 140C junction temperature thermal shutdown?
2. Figure 1 of the datasheet shows the maximum output current vs input voltage. At Vin=3V, the maximum output current is listed as ~300mA. However, using equation 1 on page 10 with the following parameters, I calculate an output current of 516mA. (Vin=3V, Vout=5V, L=1uH, f=3.75MHz, Ivalley=.7A)
-Which limit should I use for the design?
Thank you!
-Ryan